Fire suppression system for high-temperature operationsModular firefighting technology from Rescuevation based on the MiniTec profile system 25. September 2026

Today, innovative operational technology is increasingly key to efficiency and safety in firefighting. One example of this is provided by Rescuevation, which consistently relies on MiniTec’s profile system with its modular fire suppression system “SnakE 6 Professional” and customizable roll containers.

With the “SnakE 6 Professional,” Rescuevation has developed a versatile specialized fire suppression device that is used in particular for fires involving electric vehicles, as well as for wildfires and decontamination operations. The system is based on modular nozzle and hose elements that can be flexibly combined and assembled without tools.

In practice, the advantage is immediately apparent: emergency responders can set up the system in just a few minutes and adapt it to different scenarios—from underbody cooling of an electric vehicle to a mobile spray boom for wildfires. The compact design also allows for space-saving storage in standardized transport boxes.

SnakE 6 Professional is a modular fire suppression system designed to combat electric vehicle fires as well as wildfires.

MiniTec profile system as basis

A key factor in its success lies in the design: Rescuevation uses MiniTec’s modular aluminum profile system for its frames and support structures. This system is characterized by high stability, low weight, and a particularly flexible connection technology that does not require complex mechanical machining.

This offers decisive advantages, especially in the day-to-day work of firefighters: adjustments or expansions can be implemented quickly without the need for special tools or lengthy workshop time. At the same time, the design remains robust enough to withstand demanding operational conditions.

Rescuevation's fire suppression systems are based on the MiniTec modular profile system.

Benefits for fire departments

The combination of Rescuevation’s innovative products and MiniTec’s profile system creates real added value for fire departments. The modular design enables flexible, efficient, and practical solutions for a wide variety of operational scenarios. Especially in times of growing technical challenges – such as those posed by electric vehicles or an increase in wildfires – the modular principle proves to be forward-looking. 

Rescuevation impressively demonstrates how modern firefighting technology can be taken to a new level through intelligent design and a modular system. 

Would you like to learn more about MiniTec's firefighting technology? Then feel free to contact us!

Contact us