MiniTec InHouse 112Looking back on two powerful days 27. January 2026

On January 21 and 22, 2026, MiniTec InHouse 112 took place for the first time – a new event format for intensive exchange with our partners in the field of firefighting technology.

After our guests arrived on January 21 and enjoyed an evening event together at the Schlossberg Hotel in Homburg, the second day was all about meeting, exchanging ideas, and getting hands-on experience. In Schönenberg-Kübelberg, participants enjoyed factory tours, exhibition areas, and project presentations on current developments and solutions in the firefighting sector.

Our sales representatives and numerous partners took the opportunity to engage in intensive discussions, share experiences, and gain new ideas for further cooperation. The personal conversations on equal terms, honest feedback, and lively discussions quickly made it clear what MiniTec InHouse 112 is really about: trust, partnership-based cooperation, and joint forward thinking.

A big thank you to all participants for their commitment, openness, and the great atmosphere!

Here's to many more ideas and successful projects!

Do you have questions about our products and solutions in the field of firefighting technology?
Then feel free to contact us!
 

Learn more

The New Off-Road Roll Container

Designed for use beyond paved roads, the new off-road roll container impresses with sophisticated engineering and maximum off-road capability. It is based on our long-proven roll container system, which has demonstrated outstanding performance in real-world operations.

Thanks to its modular design, it offers virtually unlimited options for individual configuration and customization. Large, airless wheels with independent suspension ensure confident handling on uneven terrain. The robust aluminum frame provides absolute stability even under heavy loads. Despite its rugged construction, the container remains surprisingly agile and can be maneuvered with precision during team operations.

Learn more

MiniTec Equipment Storage for Lukas eDRAULIC Rescue Tools

A frame made from the smart MiniTec aluminum profile system that simplifies the conversion from generator-powered to battery-powered rescue tools—especially when loading them into vehicles.

By adhering to the standard dimensions of the already proven slide-out rails for hydraulic units, vehicle retrofitting can be completed in no time. The base frame extends beneath the rear centering pins and is secured using the existing locking pin. An angled plate with a slot can be precisely positioned over the T-slot system to align with the locking mechanism. Above the base frame, profiles can be adjusted, allowing the racks to be easily adapted to the tools and the available installation space.

Learn more

Customized Respiratory Protection Workshop

MiniTec draws on decades of experience in developing and manufacturing ergonomic workstation systems for industry and production. This expertise provides our specialists with the perfect foundation to cater to the individual needs of fire departments and their respiratory protection workshops.

Individual work steps—such as disassembly, cleaning, inspection, assembly, and documentation—are seamlessly integrated into the respiratory protection workshop using standardized workstation modules. These modules are adapted to create an optimal workflow that fits the available space.

Learn more