MiniTec' s new Breathing Apparatus Workshop (BAW) Extraction System sets new benchmarks in occupational health and safety. A recent reference project demonstrates how modern breathing apparatus workshops can successfully combine maximum safety with operational efficiency.
The training of breathing apparatus technicians lays the foundation for safe and professional day-to-day operations within fire services. To ensure the highest level of protection for personnel, the integration of innovative extraction solutions into breathing apparatus workshops is becoming increasingly important. The objective is clear: to prevent hazardous exposure at the workplace before it can occur.
Setting new standards for modern workshops
Today's breathing apparatus workshops are designed with a strong focus on professional, standardized workflows. MiniTec's BAW Extraction System serves as a pioneering solution, representing the current state of the art while integrating occupational health protection directly into everyday workshop operations.
A strong partnership from development to implementation
The successful market launch and the first installations were made possible through MiniTec's specialist trade partner B-A-S Brandschutz. As an experienced industry expert, B-A-S supports fire services in proactively raising workplace safety to a new level.

Vapors and aerosols are effectively extracted within the enclosure.
The solution: Certified safety through advanced airflow technology
The enclosed extraction system captures vapours and aerosols directly at their source. Perforated rear panels and additional ceiling-mounted extraction vents also remove thermally rising contaminants safely and efficiently. Thanks to a high air exchange rate, hazardous substances are diluted and discharged directly outdoors. A carefully engineered laminar airflow guides the air away from the operator at all times. For maximum operational safety, the system continuously monitors its performance. If the required exhaust air volume falls below the specified threshold, the operator is immediately alerted by both visual and audible warning signals.
Aljoscha Buch, MiniTec design engineer and firefighting expert, comments: „Hazardous substances are reliably captured within the enclosed extraction area and safely removed by a precisely coordinated exhaust air system. The laminar airflow directs the air away from the operator, while the extraction volume automatically adjusts according to the opening position of the front sliding door. This ensures maximum protection without adding any extra steps to the daily workflow..“

Everything's clean: The extraction system prevents exposure to harmful substances in the workplace.
A model for fire services nationwide
Die erfolgreiche Implementierung an Ausbildungseinrichtungen wie der unterstreicht die Relevanz dieser technischen Neuerung. Sie dient als neutrale Referenz dafür, wie technische Innovationen den Arbeitsalltag nachhaltig verbessern. Die neue MiniTec ASW-Absauglösung ist ab sofort über spezialisierte Partner erhältlich und bereit, bundesweit neue Standards im Gesundheitsschutz zu etablieren.
The successful implementation at training facilities such as the State Fire Service School Geretsried (SFS Geretsried) demonstrates the relevance of this technological innovation. It serves as an independent reference for how modern engineering solutions can sustainably improve everyday working conditions in breathing apparatus workshops. The new MiniTec BAW Extraction System is now available through selected specialist partners and is ready to establish new standards in occupational health protection for breathing apparatus workshops across Germany.
Do you have any questions or would you like to learn more about our products and solutions in the field of firefighting technology? Then please feel free to contact us!