Deflection Calculator Now Available as an AppQuickly check if your profile can handle the load 17. December 2025

When it comes to choosing the right aluminum profile for a specific application, load-bearing capacity and the resulting deflection play a crucial role. That’s why MiniTec offers a convenient online calculator, where you can enter the intended length and force in Newtons for any profile. The deflection for various load scenarios is then immediately displayed.

The calculator shows users whether the selected profile is suitable for their application. If the deflection exceeds the permissible limits, they can immediately choose a stronger component from the MiniTec modular system.

In addition to online access, mobile access via an app is naturally important for many MiniTec customers. Due to a technical update in recent months, the app was temporarily unavailable in the Google Play Store (for Android) and Apple App Store (for iOS). That is now a thing of the past: the MiniTec Deflection Calculator is once again available as a convenient app for smartphones and tablets.

Download the app directly from the following page:

 

Download the App Now