Contact us
Tel.  +49 6373 81 27 - 0
Fax  +49 0 6373 81 27 - 20
info@minitec.de

Transport trolleys

Practical helpers for intralogistics

In every company there are situations and areas where certain products, workpieces, spare parts, etc. need to be transported from A to B quickly and easily. For precisely such requirements, you will find an extensive range of transport trolleys at MiniTec. Thanks to the MiniTec modular profile system, these can be flexibly configured. Learn more

 

Transport trolley with multiple expansion options

Based on a basic trolley, a wide range of expansion options are available, for example:

  • various box superstructures
  • levels
  • Box pallets
  • Drawers
  • roller shutters and doors
  • other extensive accessories

And if you have special wishes, these can of course also be realized individually. 

Safe thanks to integrated dead man's brake

To ensure that no transport trolley "takes on a life of its own", all our products are already equipped with a so-called dead man's brake in the basic version. When the handle is released, the brake is automatically applied and the trolley stops. Incidentally, this requirement comes from the fire department, where MiniTec transport trolleys have been standard equipment for a long time. But more and more customers in industry are also taking advantage of our offering in this regard.

Back to the products